오늘 무엇을 도와드릴까요?

Configure Control Expert to communicate with the M580 through the BMENUA0100 using HTTPS.

Use the following steps for configuring Control Expert to communicate with the M580 CPU through the BMENUA0100 control port in HTTPS secure  mode.

  • Open the Security Editor.
  • Whitelist the M580 CPU certificate in the Security Editor.
  • Apply the changes.
  • Close the Security Editor.

sdcdsc

  • Open the BMENUA0100 web page.
  • Enable the IP forwarding service.

fgngf

  • Enable the HTTPS service.

eteaht

  • Disable IPSEC if it is not being used.

tgtg

  • Connect to the M580 using the BMENUA0100 control port IP address.

yrhsss

gteag