오늘 무엇을 도와드릴까요?

IGP10-T 4 and 20 mA Loop Check

  1. Press the NEXT button 3 times and CALIB will be displayed
  2. Press ENTER and CAL ATO will be displayed
  3. Press NEXT 3 times and ADJ 4mA will be displayed
  4. Press ENTER and A 4mAΔΔ will be displayed. At this time the transmitter output will be locked at 4mA.
  5. When 4mA loop check is done, press NEXT 5 times and ADJ20mA will be displayed
  6. Press ENTER and A20mAΔΔ will be displayed. At this time the transmitter output will be locked at 20mA.
  7. When 20mA loop check is done, press NEXT 6 times and CANCEL will be displayed
  8. Press ENTER and transmitter will return to measurement mode.