VarPlus Logic VL 6 - can the firmware be upgraded?
Issue
Can the firmware for the VarPlus Logic VL 6 be upgraded?
Product Line
VarPlus Logic
Environment
Firmware
Resolution
The VarPlus Logic VL6 firmware is not field-upgradable. The current firmware version is 001.000.002.
게시 대상: 슈나이더 일렉트릭 Korea