Key differences between the AP9613 and AP9614
Topic:
Key differences between the AP9613 and AP9614
Product Line:
AP9614, AP9613
Environment:
All serial number (Global)
Resolution:
The APC by Schneider Electric has released last Jan. 20, 2025 its new Dry Contact I/O card (AP9614) introducing several improvements compared to the previous model, AP9613. Dry Contact I/O card (AP9613).
- The AP9614 now includes a built‑in Web GUI, allowing users to configure UPS settings and define actions based on status changes or UPS events directly through the interface. For more information, please refer to FAQ000273840
- The AP9614 supports easy firmware updates via the Web GUI, streamlining maintenance and reducing the need for manual processes.
- The new model uses a Micro USB interface, enabling faster and more efficient data transfer, compared to the Mini USB connection used in the AP9613.
- The AP9614 can be readily identified through its updated pin configuration and internal components, offering clearer differentiation from the AP9613.
(AP9614) (AP9613)
If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.