오늘 무엇을 도와드릴까요?

video: How to use ATV Predict for Predictive Maintenance on ATV600 ?

How to use ATV Predict for Predictive Maintenance on Altivar Process ATV600 ?


➡️  Download and install EcoStruxure Automation Device Maintenance : https://www.se.com/ww/en/download/document/EADM/

➡️ Download the Altivar firmware package: Firmware package: https://www.se.com/ww/en/download/document/ATV600-Firmware/

➡️ Download  and install SoMove : https://www.se.com/ww/en/download/document/SoMove_FDT/

and the ATV600 DTM Library: https://www.se.com/ww/en/download/document/ATV6xx_DTM_Library_EN/

➡️For more information see: ATV600-ATV Predict User Manual: https://www.se.com/ww/en/download/document/NAT10588/

🔔 Timestamps:
00:29 – Purchase and install ATV Predict license
00:47 – Connect to the drive via webserver
01:00 – License activation with SoMove
01:48 – Commissioning wizard setup
02:14 – Configure motor parameters
02:59 – Configure sensors (pressure, flow)
04:30 – Configure pump and curves
05:20 – Validate setup and launch diagnostics
05:45 – Real-time KPI monitoring and cavitation detection