Is CPU over-clocking with Turbo-boost available for PSA6?
Yes, the default setting is Turbo-boost enabled. It can be disabled from the BIOS menu.
When Turbo-boost is turned on for PSA6 with Core i5 CPU, it is recommended to use a power supply with at least 80% higher capacity than the specified power consumption.