오늘 무엇을 도와드릴까요?

Default Login Credentials for Sage RTU C3414 Red CPU

Title:
Default Login Credentials for Sage RTU C3414 Red CPU (Secure Firmware)

Issue:
Unable to access the Sage RTU C3414 (Red CPU) due to unknown or forgotten login credentials.

Product:
Sage RTU C3414 – Red CPU variant (Secure Firmware)

Environment:
Device: Sage RTU C3414 CPU
Access Method: Web interface or serial console
User Role: Administrator

Cause:
The device requires valid login credentials for access. Users may not be aware of the default credentials set by the manufacturer.

Resolution:
Use the following default credentials to log in:

  • Username: Admin
  • Password: Telvent1!

⚠️ It is recommended to change the default password after initial login to ensure system security and prevent unauthorized access.