LV429337T, LV426930T : 비상시 도어 오픈 가능한가요?
Ref: LV429337T(NSX) vs LV426930T(NSXm)
With reference to your query we wish to inform you that for Both LV429337T(NSX) and LV426930T(NSXm) , The rotary handle is delivered with the door lock deactivated. It is recommended to activate the door interlock .
When the door lock is activated, the rotary handle locks the door when the handle is in the I-On or Trip position, the door interlock activates once the Handle moves from OFF position towards ON Position.
Only qualified persons are authorized to disable the door lock, when the MCCB is in ON or in Trip position , it can be done with a simple screw driver as mentioned in the instruction sheet attached .
LV426930T(NSXm) to inhibit door locking in the I-On position, turn the screw , situated under the door locking mechanism, 10°–15° clockwise.
LV429337T(NSX) To inhibit door locking in the I-On position, turn the screw , situated under the door locking mechanism,90° anticlockwise.
NSXm (LV426930T): 잠금 해제를 위해 도어 잠금 장치 하단의 나사를 시계방향으로 약 10~15° 회전
NSX (LV429337T): 잠금 해제를 위해 도어 잠금 장치 하단의 나사를 반시계방향으로 약 90° 회전