오늘 무엇을 도와드릴까요?

PME - Designer diagram doesn't open "This node is locked by DESIGNER.SERVERNAME"

Issue

In PME, opening a VIP or ION meter using Designer displays the following error: "This node is locked by DESIGNER.SERVERNAME. Please try again once the node has been released."

This node is locked by DESIGNER

Product Line

Power Monitoring Expert

Environment

Designer

Cause

Another instance of Designer is running and currently has the VIP or ION meter open.

Resolution

Note: if the error message says "LOGINSERTER.SERVERNAME" instead of "DESIGNER.SERVERNAME", the PME log inserter component is uploading records from the VIP or ION meter. Wait for it to be automatically released once finished; it may take several minutes or over an hour depending on the number of records and connection type.

If the error message shows the server name (DESIGNER.SERVERNAME) there is another user logged into the server that has that node open in Designer. The other user will need to close the node's diagram in Designer to release it. Alternatively, follow the steps below to find and close all instances of Designer using Task Manager:

  1. Open Task Manager > Users.

Task Manager users

2. Click the arrow next to a user to view open processes in their session. Right-click on each instance of Desginer.exe > End task.

End task of instances of Designer.exe under users

If the error message shows a different computer name (DESIGNER.COMPUTERNAME) connect to that engineering client computer and close Designer.

If unable to track down the other instance of Designer, reboot the application server.