오늘 무엇을 도와드릴까요?

Is it possible to monitor the Primary and Standby PLC state of the M580 redundant system via the Ecostruxure OPCUA Server Expert?

Issue:

Monitoring the Primary and Standby PLC state of the M580 HSBY system via the Ecostruxure OPCUA Server Expert 2.1.4906 SP3


Product Line:

Ecostruxure OPCUA Server Expert


Resolution:

Yes, it is possible via the "#DeviceServiceLevel computation" option in the OPCUA Server Expert configuration. To enable, launch the configuration tool and go to the "communication"  settings and check the "Extended rules" .

image2

image1