Issue:
Where can I confirm if the ATS48 is compliant with Lloyds Register or DNV?
Product Line:
ATS48, Altistart 48
Environment:
All
Cause:
NA
Resolution:
ATS48 is compliant to Lloyds Register .
The certificate is attached to this document.
Concerning DNV, the ATS48 is compliant to DNV.
The certificate is available on DNV website, at link:
https://approvalfinder.dnv.com/TAE00001AZ?filterMode=both&searchText=TAE00001AZ
Опубликовано для: Schneider Electric Казахстан