Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
ATV340 -When setting up the drive, using Somove, how do I assign a Preset speed to a digital input?
Issue:
How do I assign a Preset speed to a digital input, in Somove?

Product Line:
Software

Environment:
Somove

Cause:
In the I/O menu digital input assignments are grayed out. Unable to change.

Resolution:
To setup Preset speeds:
Go to the Preset speed function and assign the desired digital input.