PM5111 meter is MID compliant. As per the requirement of the MID standard, the energy pulsing is fixed based on the PT and CT secondary values. So, the user is not allowed to configure the energy pulsing for LED in MID references. This is why the LED configuration option is not available in the PM5111 meter.
Опубликовано для: Schneider Electric Казахстан