Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Is there an isolation between 24V and S485 port of ATV212?
Issue:
Is the RS485 port of ATV212 isolated from the internal 24V supply on the VFD?

Product Line:
ATV212

Environment:
All

Cause:
To avoid potential damage to the RS485 port when running long distance.

Resolution:
No, the RS485 port is not isolated from the internal 24V supply on ATV212.