{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can we use one VW3A1101 keypad on multiple ATV212 drives?
Issue:
Using VW3A1101 keypad on multiple ATV212 drives.

Product Line:
ATV212

Environment:
Keypad

Cause:
n/a

Resolution:
Response from France:

The VW3A1101 keypad used on ATV212 is just like a mirroring display with a long label. You can see it because; the local ATV212 display will change in the same time, that the keypad displays.

VW3A1101 keypad + ATV212 does not offer the same characteristics (configuration saving, Multidrop, HMI personalization, menu organization, etc.),  like with  VW3A1101 + ATV320 or ATV61 or ATV71.

So the Multidrop/Multipoint is not possible with the ATV212 and VW3A1101.

There is a mistake in the catalog. Request has been made to correct it ( 1/2/19).

Schneider Electric Nigeria

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: