Our Brands
Welcome to the Schneider Electric Website
For Cybersecurity reasons use the following versions ILA2x Drive Firmware (PR892.30) - V01.103 (or greater) ILx2T Modbus TCP Communication Firmware (PR907.30) - V01.107 (or greater) ILx2K EtherNet/IP Communication Firmware (PR907.40) - V01.107 (or greater) ILx2T Modbus TCP Product Manual - 08/2020 (or greater) ILx2K EtherNet/IP Product Manual - 08/2020 (or greater) Lexium CT - V2.010 Release 1/27/2011 (or greater) GDB File - blct089x30_01103.gdb (or greater) To update your device contact your local Schneider Electric representative.
Files
Related products
Product Ranges: