Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Number of cables can be terminated in to transformer mounted 1250A MCCB cabinets.
Transformer mounted MCCB cabinets rated 800A & 1250A can terminate up to 7 single core 600mm cables as standard, (using single M16 holes).
Alternative arrangements can be applied on request (please consult Schneider Electric).

Schneider Electric Netherlands

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: