Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an PHF input phase fault ( error ) on the ATV61 and ATV71 drives?

Article available in these languages: Dutch

Product Line:
ATV61 ATV71

PHF: input phase loss

Principal:
This fault appears when an input phase is lost.
If 2 or 3 phase disappears while the drive is running, the drive will continue to run until the drive trips in another fault (USF for example).

This function could be disable by software with the parameter IPL=NO to supply the drive via the DC BUS voltage (range 230V and 480V).

Some drives (230V up to 7,5kW) have IPL=NO in factory setting because they can be supply in single phase.


Be careful, In the case where the motor is in generator mode then the fault doesn’t appear.
Be careful, the fault is stored in the EEPROM during a run.

Probable cause:
- Drive incorrectly powered or fuse opened.
- Loss of one input phase.
- Use of a single-phase input on a three-phase 200...240VAC ATV71 of ATV61.

Remedies:
Check the power connections and the fuses.
Use a three-phase distribution network.

Inhibit the IPL fault (input phase loss) as follows:

Menu [1.8 FAULTMANAGEMENT] ( FLt- )  parametergroup iPL- by setting subparameter iPL to  [ Ignore ] ( no )
Input phase fault is now ignored, to be used when drive is supplied by single phase supply or DC bus.


Schneider Electric Netherlands

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: