Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Could auxiliary contacts (i)OF for iC60/C60 be used for DC voltage above 130VDC?

Article available in these languages: Dutch

Auxiliary contacts (i)OF for Acti9 iC60 / Multi9 C60 has operating voltage up to 130VDC (or less for some references).
Disconnecting of DC currents is technically much more difficult than AC currents (which crosses zero level in each period).
An electrical arc is generated during disconnection (opening).
Ability of contacts to break this arc depends on DC voltage, current, distance of contacts in open position and material of contacts.
The current through aux. contacts for iC60/C60 are not tested and certified for  disconnection of DC voltage over 130VDC.
So therefore we cannot recommend such usage.

Schneider Electric Netherlands