Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Masterpact MTZ have the same dimensions like NW / NT ?

Article available in these languages: Dutch, Thai

YES, MTZ keeps the same height and width with the one of current NT / NW breaker, the depth will be slightly increased for 3mm for both the fixed and the withdrawable version.

This 3mm increase is only at the front cover level, the baseline of the breaker basic frame is not changed.

Normally it won’t pose any problem to integrate MTZ into the current switchboard, no part needs to be modified in Prisma, Blokset or Okken cubicle.

Schneider Electric Netherlands