Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Masterpact MTZ have the same electrical characteristics like Masterpact NW/NT?

Article available in these languages: Dutch

The product range Masterpact MTZ has the same electrical performance with Masterpact NT/NW. Nevertheless, a new performance H3 on the small frame size (MTZ1) is added.
Purpose is to improve the Rated Short-time Withstand Current Icw up to 50kA/1s for the small frame.

Schneider Electric Netherlands