Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the panelbuilder obliged to re-certify the switchboard with Masterpact MTZ as per IEC 61439 ?

Article available in these languages: Dutch

For most of the customers the substitution of NT/NW circuit-breakers by MTZ123 can be performed without recertifying the switchboard.
Schneider Electric provides attestation documents from third party certification companies to confirm that according to IEC 61439,
there is no need for re-certify the switchboard when replacing Masterpact NT/NW by Masterpact MTZ1/2/3.

Nevertheless,
- For certain customers, especially Panelbuilders dedicated to specific applications ( e.g Oil &Gas ) may have to re-test or re-certify their switchboard with MTZ.
- An update of existing certification is required to integrate the newly added performance MTZ1 H3.

Schneider Electric Netherlands