Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SoMove conversion ATV61/71 to ATV600/900 possible ?

Article available in these languages: Dutch

It is not possible to convert SoMove files ATV61 and ATV71 to ATV6*0 or ATV9*0
This will have to be done manually by creating a new SoMove file with the settings
which are changed against factory settings from the SoMove file of the ATV61 / ATV71.

Schneider Electric Netherlands