Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the substitution / alternative for Integral 18 & 32 motor starters.

Article available in these languages: Dutch

The Integral 18 & 32 motor starters are discontinued ( obsolete ) now, the nearest correct substitute is Tesys U motor starter.
Please note that Tesys U is a customized product & one has to order following references as per the requirement

1) Power Base
2) Control Unit
3) Function modules/Communication modules/Auxillary contact modules
4) Auxillary contacts
5) Reverser block
6) Plug-in terminal blocks
7) Control circuit pre-wiring system

Cross reference guide for your reference and catalog TeSys U is attached below

TeSys U
To the product selector TeSys U motorstarters ( dutch version ) >>

Schneider Electric Netherlands

Attachment(s)
Cross References Integral to TeSys U.xls [197 KB]
A4 - TeSys U refs.pdf [16.7 MB]