Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Altivar - What are possible causes for nSt status ?

Article available in these languages: Dutch

Product Line:
Altivar ATV Drive line

Display code nSt is a drive freewheel state.  It is not a fault.  If the drive is in an nSt state you can not run the drive in local or remote mode.

1:) 3 wire control:  check to see if  NC stop on LI1 is open to +24vdc.
2:) 2 wire control:  check to see if the 2 wire type is level control or check to see if there is a run command on LI1 during power up.
3:) nSt assigned as an logic input and that input is open.
4:) Stop button has been pushed on the local face or remote HMI and the drive is being commanded in terminal mode.
5:) Drive is an CIA402 (DSP402) drive com NET command mode and is not received the proper commands to go to the rUn  or rdY state.
6:) Any drop in +24V supply on the drive can cause nSt.

Schneider Electric Netherlands