{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can I connect a busbar trunking system of the KBB25A type with a KBB40A?
Yes, you can connect a busbar trunking system of the KBB25A type directly to a KBB40A.
They are fully compatible, in terms of both mechanical and electrical connections.

Caution: The complete line then becomes a 25 A line.

Schneider Electric Netherlands

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: