Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Differential Circuit breakers for 110VAC network
Some differential breaker will work on 110VAC and trip when a fault occurs however,
According to the standards you need to have a working test button always, not only most of the times.
For that reason we propose specific references for 110V applications: See attachment.

Schneider Electric Netherlands

Attachment(s)
110V Differential Modular Breakers.pdf [71.15 KB]