Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What will cause an Altistart ATS46 or Altistart ATS48 to generate error FrF (Frequency Fault)?
Product Line:
Altistart ATS46/ATS48

Possible Cause:
• Error FrF is caused by mains supply frequency is outside acceptable limits.

Corrective Action:

The softstarter is by default set ( parameter FrC in menu drC ) to AUt ( 50/60Hz +/- 5% )
Check that the frequency is between:
• 50 Hz +/- 2.5 Hz (47.5 Hz to 52.5 Hz)
• 60 Hz +/- 3.6 Hz (56.4 Hz to 63.6 Hz)


If the main supply frequency is out of above tolerance, the parameter FrC can be set
to 50 or 60Hz the guarded tolerances will become  50Hz +/- 20% or 60Hz +/- 20%


If above does not solve the problem, check the internal connections in the softstarter.
If they are all ok, then suspect a problem with the ATS46 or ATS48 Main Control Board .
The ATS46 Main Control Board is no longer available and the  softstarter has to be replaced with
An  ATS48 – series softstarter.  The ATS48 Main Control Board part number is VX4G481

Schneider Electric Netherlands