Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to install a Harmony XB4 potentiometer correctly

Productgroup
Harmony XB4

Purpose
Install an XB4 potentiometer correct correctly.

Solution
On below video an instruction to assemble the parts of the potentiometer ( covercap, turning head, mountingflange and potentiometer) easily.
Tools: screwdriver 5,5 x 125mm, Philipspoint screwdriver 0 x 75mm


When you use a complete Schneider assembly (Head and Potentiometer delivered together) the electrical connections A,B and C and picture of the circuit are printed on the circuit board above the screw connections.

Schneider Electric Netherlands