Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set up commandswitching via logic input on ATV630 and ATV930 drives?
How do you set up a command switch via logic input on the ATV630 and ATV930 drives?

Product Line:
Altivar Process ATV630 and ATV930 drives

Environment:
All

Cause:
Need to use a logic input to switch between two command functions like HMI start stop and terminal start stop.

Resolution:
Programming
Press the Home button.
Scroll down to menu 5 complete settings enter.
Scroll down to menu 5.5 command and references enter
Scroll down and choose command switching and assign it to DI3 enter
Scroll down and choose CMD channel 1 for your first command and CMD 2 for your second command.


Schneider Electric Netherlands