IP-based Building Systems Network from Cisco and Schneider Electric
Cybersecure and Efficient Network Technology Solution The Cisco-Schneider solution is unlike other building automation offers because it is built on IP protocols and an open integration platform. This allows it to gather information from a broad range of sources—connected room sensors and third-party building services, for example—and send it to a cloud analytics platform and workplace management applications.
Fecha:
01 jun 2018| Tipo:
Promocional
idiomas:
Inglés| versión:
1.0
Referencia del documento:
IP-based-Building-System-Cisco