Search FAQs
How to enable the Vijeo Designer Runtime to launch automatically on an iPC?
Issue:
Vijeo Designer Runtime does not launch automatically when Windows reboots.
Product Line:
Magelis iPC or HMIG5U/HMIG5Us with Vijeo Designer Runtime
Cause:
The Vijeo Designer Runtime Manager provides the ability to enable or disable Autostart for Vijeo Designer Runtime. It is likely the setting has been changed from the factory state.
Resolution:
On the desktop, look for the gray icon labelled "Vijeo Designer Runtime Manager". Launch the application (by right-clicking and "Run as Administrator"). Set the setting to Enable AutoStart so that Vijeo Designer Runtime will start when Windows launches.
Note: If your iPC has an EWF (Enhanced Write Filter) protected system volume, be sure to unlock it first.
Vijeo Designer Runtime does not launch automatically when Windows reboots.
Product Line:
Magelis iPC or HMIG5U/HMIG5Us with Vijeo Designer Runtime
Cause:
The Vijeo Designer Runtime Manager provides the ability to enable or disable Autostart for Vijeo Designer Runtime. It is likely the setting has been changed from the factory state.
Resolution:
On the desktop, look for the gray icon labelled "Vijeo Designer Runtime Manager". Launch the application (by right-clicking and "Run as Administrator"). Set the setting to Enable AutoStart so that Vijeo Designer Runtime will start when Windows launches.
Note: If your iPC has an EWF (Enhanced Write Filter) protected system volume, be sure to unlock it first.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: