Search FAQs
Smart-UPS On-Line with Li-Ion batteries reports "Error B.08" or inaccurate runtime
Issue: Smart-UPS On-Line with Li-Ion batteries reports "Error B.08", or shows inaccurate runtime remaining on the UPS LCD display, when XBP48RM2U-LI battery pack is connected.
Product Line: SRTL1000RM4UXLI, SRTL1000RM4UXLI-NC, SRTL1500RM4UXLI, SRTL1500RM4UXLI-NC, SRTL1000RMXLI, SRTL1000RMXLI-NC, SRTL1500RMXLI, SRTL1500RMXLI-NC, SRTL2200RM4UXLI, SRTL2200RM4UXLI-NC, SRTL3000RM4UXLI, SRTL3000RM4UXLI-NC, SRTL2200RMXLI, SRTL2200RMXLI-NC, SRTL3000RMXLI, SRTL3000RMXLI-NC
Resolution: This is addressed in UPS firmware version 15.3.
Restart the UPS, then update the UPS firmware to the latest version. Refer to FA16473, FA279197 or FA170679 to update the UPS firmware.
Product Line: SRTL1000RM4UXLI, SRTL1000RM4UXLI-NC, SRTL1500RM4UXLI, SRTL1500RM4UXLI-NC, SRTL1000RMXLI, SRTL1000RMXLI-NC, SRTL1500RMXLI, SRTL1500RMXLI-NC, SRTL2200RM4UXLI, SRTL2200RM4UXLI-NC, SRTL3000RM4UXLI, SRTL3000RM4UXLI-NC, SRTL2200RMXLI, SRTL2200RMXLI-NC, SRTL3000RMXLI, SRTL3000RMXLI-NC
Resolution: This is addressed in UPS firmware version 15.3.
Restart the UPS, then update the UPS firmware to the latest version. Refer to FA16473, FA279197 or FA170679 to update the UPS firmware.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: