Issue
Does the BMXAMI0800 or BMXAMI0810 require an external loop power supply or does the module provide it for the 4-20mA current loops ?
Product line
Modicon X80 IO
Resolution
Yes. Both the BMXAMI0800 and BMXAMI0810 require an external loop power supply for their 4-20mA current loops. The module does not provide it.
Publicerad för:Schneider Electric Sverige