What is the ACE917?

Product Line
LPCT
ACE917

Environment
Testing

Resolution
The ACE917 is an adapter that is used to test the protection chain using as standard injection box, when the SEPAM relay is connected to LPCT APS_SENSORS.
Attached is the manual for the ACE917

ชไนเดอร์ อิเล็คทริค Thailand

เอกสารแนบ
LPCT type current sensors.pdf [182.81 KB]