Viewing and Clearing P1.Log (Priority 1 / High Priority) Alarms from the CM2000 Front Panel

Issue
End User sees "P1.Log: displayed on the screen of a CM2000 (which is shown the the picture below) and would like to clear this alarm.

CM2000

Product Line
CM2000 series

Environment
PowerLogic Power Meters

Cause
The limits set for a high priority alarm has been exceeded and tripped the alarm.

Resolution
Please follow the procedure below to clear the alarm.


Procedure
1. Press the MODE button until the red LED next to ALARM glows steadily. The circuit monitor
displays P1.Log.
2. Press the Enter button to see which P1 alarms have not yet been cleared. To see if there is more
than one P1 alarm, press the blue arrow buttons. It will list different P1 alarms as you press the
button.
3. Press the Enter button one time, and CLEAr should be displayed.
4. We want to go into CLEAR Mode, so press the Enter button ONCE. The circuit monitor displays
CLr. No.
5. To clear the log, press the up arrow button to change from CLr. No to CLr.YES. Then press the
Enter button. The circuit monitor clears the P1 Log, and releases any latched relays IF THE
ALARM IS not STILL ACTIVE.
6. After clearing the P1 Log, the display should read AL.CodE. Press the Enter Button to verify
there are no active alarms (it will say NONE-).
7. Press the Enter button again to go to the P1.Log. Press Enter and the P1 Log should also say -
NONE-.

ชไนเดอร์ อิเล็คทริค Thailand

ดูข้อมูลเพิ่มเติม
รุ่น:
บทความที่อาจช่วยได้
ดูข้อมูลเพิ่มเติม
รุ่น: