Issue:
CLr code meaning on ATV212 and how to clear it.
Product Line:
ATV21, ATV212
Environment:
All range, All serial number
Cause:
Need to reset the VFD.
Resolution:
This code shows up when someone presses the Stop key in front of the drive while another fault is displayed. To clear this code, press the stop button again or power cycle the drive.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand