A Product Environmental Profile (PEP) is a quantitative Type III Environmental Declaration in compliance with ISO 14025 which ensures appropriate reliability and transparency. Based on a life cycle assessment (LCA) of the product along its whole life cycle, the document presents the different impacts such as energy consumption, carbon footprint, consumption of raw materials, and pollution of air, water, and soil.
Check out more information on the Schneider Electric Environmental Data Program.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand