How to Pair the Zigbee MicroLogic Active Control Unit with Panel Server - MasterPacT MTZ
When installing a MasterPacT with a Zigbee MicroLogic Active control unit, discover how to pair the control unit with a Panel Server (PAS). This will require a PC with an Ethernet connection to the PAS. Next, connect to the PAS's webpages and search for wireless devices. After putting the control unit in pairing mode, it will be automatically detected by the PAS.
日期:
25 11月 2024|類型:
教學影片
語言:
英語|版:
1.0
子類型: 功能與應用, 安裝細節, 系統設計, 故障排除
參考文件:
Masterpact-MicroActiv-Pair
系統提供的線上文件均為最新版本。 檔案
檔案名稱
Video04-How to Pair_MicroLogicActive_with_PAS_MasterPacT_HD_1.mp4