Issue
The purpose of this Resolution is to inform Advantys users that the Ethernet NIM web page Exec has been updated to version 1.18.
Product Line
Advantys STB
STBNIP2212
Environment
Resolution
Upgrading the STBNIP2212 Ethernet NIM web pages to version 1.18 adds support for the following modules:
- ATV71 (with Advantys Configuration software version 2.51)
The attached zip file contains:
- NIM web Upgrade Procedure 1.18.doc
- upgrade.exe
- web_files.zr
Please read the 'NIM web Upgrade Procedure' before attempting to load the web file.
發佈於: 施耐德電機Taiwan