Issue
Which firmware revisions are supported in each rack PDU/ATS model?Product Line
- Rack ATS (AP77xx, AP44xx)
- Rack PDU (AP78xx(B), AP79xx(B), AP8xxx)
Environment
- All firmware versions (unless otherwise specified)
Cause
This compatibility chart has been created for reference.
Resolution
Please refer to the table below.
Model | Firmware app name | NMC Generation |
AP78xx, AP79xx | rpdu | NMC1 |
AP84xx, AP86xx, AP88xx, AP89xx, AP78xxB, AP79xxB | rpdu2g | NMC2/NMC3 after mid-2022 |
APDU9xxx | rpdu2g | NMC3 |
AP7701, AP7750, AP7722 | ats | NMC1 |
All other AP77xx models | g2ats | NMC1 |
AP44xx | ats4g | NMC2 |
AP44xxA | ats5g | NMC3 |
發佈於: 施耐德電機Taiwan