Yes, it is possible to install the Fusarc fuses in the upstream of Load Break Switch (LBS) switch.
Note:
1. Refer the attached sheet to choose and install the right fuse.
2. The current rating for the Fusarc Fuses has also been provided in the attached document.