Issue:
When a Type B UPS goes on battery in a Simple Signaling configuration with an Interface Expander 2 card using Timer Mode, the simple clients gracefully shut down after the configured time, but the Controller server does not.
Product:
PowerChute Business Edition v9.5 and above
Environment:
Simple Signaling with Interface Expander 2 card (AP9624) and Type B UPS devicesSolution:
To work around this issue:
- Option 1: Reset the DIP switch on the Interface Expander 2 card from “Timer Mode” to “Confirmed Mode” (0000) for Type B UPS devices, and configure all PowerChute clients (Controller and simple) to shutdown at “After the UPS has been on battery for” in the Shutdown Settings screen. This is the same as Timer Mode but is configured in PowerChute.
- Option 2: You can configure a command file to shut down the Control server for the “On Battery” event in the Event Configuration screen, which ensures a graceful shutdown. However, the Control server will still shut down if the power outage does not last 2 minutes (Timer Mode setting on the Interface Expander 2 card).
Опубліковано для: Schneider Electric Україна