Item count in basket is 0 Help and Contact Centre Item count in basket is 0 My Products Item count in basket is 0 My Documents

Our Brands

Register today
  • Get custom product tools and services
  • Access training
  • Manage support cases
  • Create and manage your orders (authorised partners only)
Log in Create account Read more benefits
SE logo LIO white header
0 item count of documents is
Impact-Company-Logo-English Black-01-177x54
Help and Contact Centre Item count in basket is 0 My Products Item count in basket is 0 My Documents Item count in basket is 0 Login/Register opens in new window
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
  • About us
  • Newsroom
  • Details

  • Home
  • News & Press Releases
  • Spokespeople
  • Assets
  • Blog
  • Contact us

Schneider Boosts Next Generation TeSys Giga Offering with Digital Innovation

digital innovation

13/04/2021

Schneider Electric, the leader in the digital transformation of energy management and automation, today announces the release of new generation of TeSys Giga series Motor Starters.

The iconic TeSys Giga series has been reimagined with the latest smart digital innovations to deliver a simpler, more sustainable, safe and secure customer experience for panel builders, consulting engineers, system integrators, facility managers and original equipment manufacturers (OEMs) further building on proven reliability and high electrical durability.

With 56 patents under the belt, TeSys Giga series Motor Starters is designed to serve the needs of the process machinery, water and wastewater, metals, minerals and mining as well as various manufacturing and processing industries. It reduces engineering time and complexity, whilst improving machine reliability and driving down maintenance costs, reducing downtime through a number of unique benefits and features:

  • Modular design: The unique set up enables easy replacement of spare parts, improving the reliability and robustness by up to 90% with up to 50% faster integration and commissioning time.
  • Compact footprint:  Compact design with 40% size reduction to enable optimal cabinet installation space.
  • Self-diagnosis: Predictive maintenance can be achieved through contact wear diagnostic and coil over/under voltage detection. A unique calculation method provides a more precise status, significantly reducing the downtime and optimizing site operation with tips wear level indicator, coil under/over voltage indicator, internal fault indicator, and contactor open & close status indicator. This feature significantly maximizes resilience and uptime for an efficient site operation.
  • Full-scale protection: Initial settings guarantee a safe customer journey when it comes to overload relay protection, including overload protection, ground fault protection, and phase imbalance protection.
  • QR Codes: Delivers technical documents, technical video guides, and counterfeit safeguards which improve customer experience.
  • Highly reliable and ready for harsh environment: Improved auxiliary contacts (17V,1mA,10-8) enable better reliability in harsh environment and conform to high density PLC input applications

“We are proud to continue delivering ground-breaking digital innovation addressing our customers’ most pressing needs,” said Nadège Petit, EVP Power Products at Schneider Electric. “In today’s rapidly changing world, it is important to equip the industry with full control over the safety and reliability of mission-critical operations, with the ability to detect and resolve faults at pace. What’s more, we want to enable a streamlined and optimized manufacturing process with solutions that are safe, reliable and interoperable. We are delighted that machine builders and panel builders can now maximize efficiency with faster machine integration, and system integrators can enjoy a more solution-oriented service.”

Contact press

UK and Ireland Press Office

UK and Ireland Press Office

+44 207 802 2626
schneideruk@teamlewis.com

Adoption of Wiztrust's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page: