Issue:
What is the part number of the fuse base for the Class 9422 Type TEF10 disconnect switch?
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
Class 9422 Disconnect Switches
Resolution:
40566-028-51. Note fuse clips are not replaceable so if needed the complete fuse base must be replaced.
What is the part number of the fuse base for the Class 9422 Type TEF10 disconnect switch?
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
Class 9422 Disconnect Switches
Resolution:
40566-028-51. Note fuse clips are not replaceable so if needed the complete fuse base must be replaced.
Released for:Schneider Electric USA