Issue:
Repair parts
Product Line:
Combination Service Entrance Device
Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056236050 (meter cover/utility pullbox cover)
Meter Cover Mounting Wing Nuts (4) 2350102000
Main Breaker Section Cover - 4056258950
Main Breaker Section Cover Mounting Screws - (3) 2142217101
Interior Deadfront Trim - 7329420650
Interior Deadfront Trim Mounting Screws - 4020513001K (10 screws; only 6 required)
Interior Deadfront Trim Handle - (1) 2940101103 and Rivets (4) 2430315290
Meter Base Assembly - 4056257050
Mounting Channel - 4056142003
Repair parts
Product Line:
Combination Service Entrance Device
Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056236050 (meter cover/utility pullbox cover)
Meter Cover Mounting Wing Nuts (4) 2350102000
Main Breaker Section Cover - 4056258950
Main Breaker Section Cover Mounting Screws - (3) 2142217101
Interior Deadfront Trim - 7329420650
Interior Deadfront Trim Mounting Screws - 4020513001K (10 screws; only 6 required)
Interior Deadfront Trim Handle - (1) 2940101103 and Rivets (4) 2430315290
Meter Base Assembly - 4056257050
Mounting Channel - 4056142003
Factory Installed Main Breaker - LJL36400U31X (mounting kit S36967 is also required; lugs on the ON end of the breaker must be removed for connection to the busbars; B phase (center) lug should also be removed from the OFF end of the breaker)
Utility Lug Mounting Hardware - 4056211850
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.
Utility Lug Mounting Hardware - 4056211850
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.
Released for: Schneider Electric USA