Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Why do I have different Line-To-Ground Voltages with my Isolated Power System?
Issue:
Different Line-To-Ground Voltages on Isolated Power System

Product Line:
Hospital Isolated Power Systems

Environment:
NFPA 99, NEC 517.160

Resolution:
Except for rare occasions, the measured line-to-ground voltage quantities will not be equal for several reasons:

1. The proximity of each (L1 and L2) conductor to ground will be different when running the wires in conduit; therefore, the line-to-ground capacitance will also be different. Running twisted pairs of conductors (which are twisted) at roughly 2-foot intervals is a good approach for achieving symmetrical line-to-ground capacitances.

2. Not all circuits have loads that can be turned ON and OFF with DPST (double pole single throw) switches; therefore, loads with SPST (single pole single throw) switches that are in the OFF state add to the line-to-ground capacitance between only one of the isolated power conductor and ground.

3. Loads are often designed to be powered from a grounded, instead of an isolated, supply. A line-to-ground filter is often added between the HOT wire and ground. This approach for attenuating electrical noise further adds to the asymmetry between line-to-ground capacitances.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings