undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the MP Meter-Pak or EZM meter centers available with a NEMA 4/4X stainless steel enclosures?
Issue:
Product Design

Product Line:
Meter Pak and EZM Metering

Resolution:
No, the MP Meter Pak or EZM Metering devices are NOT available in a NEMA 4/4X design, nor are they available in stainless steel. They are ONLY available in a painted, galvannealed steel, NEMA 1/3R construction.

Schneider Electric USA

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: