Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Schneider Electric East Africa introduces new PrismaSeT power distribution switchboard range for smart energy management

Schneider Electric, the global leader in energy management and automation, and recognised sustainability leader, is proud to introduce its next-generation PrismaSeT range of power distribution switchboards to the East African market.  

 

The range, which includes the PrismaSeT G and PrismaSeT P models, is well suited to region’s growing demand for future-ready energy management across key sectors like manufacturing, commercial real estate, data centres, hospitals, and critical infrastructure.  

 

The PrismaSeT G is a compact wall-mounted or floor-standing unit, rated up to 630A and 25kA, making it ideal for mid-sized commercial and light industrial applications. The larger PrismaSeT P model is floor-standing, rated up to 4,000A and 100kA, a powerful solution for energy-intensive industries, large facilities, and data centres. 

 

“East African businesses increasingly require smart, scalable, and safe electrical infrastructure to support rapid growth and ensure business continuity,” says Geraldine Sande, Channel Sales Leader at Schneider Electric East Africa. 

 

“The PrismaSeT range offers a robust, modular switchboard system that helps our customers improve operational efficiency, reduce downtime, and adapt easily as their energy needs evolve.” 

 

Tailored for dynamic industries 

 

The PrismaSeT switchboard system is fully type-tested to ensure high reliability and operator safety, a critical factor in sectors like healthcare and hospitality, where uninterrupted power is essential. Its strong, reinforced frames offer superior mechanical durability, even in harsh operating environments such as manufacturing plants or mining sites. 

 

An important differentiator of the PrismaSeT range is its built-in cloud connectivity. Facility managers and maintenance teams can therefore access real-time data on power usage, receive smart alarms, monitor system health, and detect voltage loss, all from a connected dashboard. 

 

“This connectivity enables more proactive energy management, supports preventative maintenance, and gives facility managers the tools to reduce operating costs and energy waste,” explains Sande.  

 

“For example, in East Africa’s expanding data centre sector, this visibility and uptime assurance are essential for supporting critical services,” she adds. 

 

Additionally, PrismaSeT panels can be equipped with HeatTag, Schneider Electric’s AI-driven fire prevention solution. HeatTag monitors the chemical changes in air inside the switchboard, identifying early signs of cable overheating before traditional temperature sensors can detect a problem. 

 

Fast and flexible assembly 

 

The PrismaSeT boards are designed with predefined mounting and front plates that align with Schneider Electric’s circuit breakers. Installers no longer need to drill or modify components, reducing installation time by an average of 20% compared to conventional boards. 

 

This modularity not only speeds up installation but also supports future upgrades. As business operations expand or change, the switchboards can be easily reconfigured to accommodate new requirements without needing to replace the entire unit. 

 

“This flexibility is particularly valuable in the region’s fast-growing economies, where commercial and industrial projects are constantly evolving,  Our PrismaSeT series enable users to scale their infrastructure cost-effectively and sustainably.” 

 

The PrismaSeT series technical features include: 

 

 PrismaSeT G 

  • Supports low-voltage power distribution up to 630 A.
  • Modular design for quick installation and easy expansion.
  • Engineered to operate safely in high-stress environments.
  • Offers a range of protection ratings (IP30 to IP55) for various settings.
  • Compatible with Schneider Electric’s HeatTag fire prevention sensors.
  • Seamlessly integrates into Schneider Electric’s EcoStruxure IoT architecture for smart monitoring. 

 

 PrismaSeT P  

  • Handles demanding installations with capacity up to 4000 A.
  • Built to withstand peak electrical loads and harsh conditions.
  • Flexible configuration with advanced modularity for large-scale facilities.
  • Enables predictive maintenance through wireless sensors and LPWAN connectivity.
  • Fully equipped for integration with Schneider Electric’s HeatTag and PowerLogic systems.
  • Designed for sectors prioritising uptime and operational efficiency. 

 

End

 

About Schneider Electric 

Schneider’s purpose is to create Impact by empowering all to make the most of our energy and resources, bridging progress and sustainability for all. At Schneider, we call this Life Is On.

 

Our mission is to be the trusted partner in Sustainability and Efficiency.

 

We are a global industrial technology leader bringing world-leading expertise in electrification, automation and digitization to smart industries, resilient infrastructure, future-proof data centers, intelligent buildings, and intuitive homes. Anchored by our deep domain expertise, we provide integrated end-to-end lifecycle AI enabled Industrial IoT solutions with connected products, automation, software, and services, delivering digital twins to enable profitable growth for our customers

 

We are a people company with an ecosystem of 150,000 colleagues and more than a million partners operating in over 100 countries to ensure proximity to our customers and stakeholders. We embrace diversity and inclusion in everything we do, guided by our meaningful purpose of a sustainable future for all

  

www.se.com  

 

Adoption of Wiztrust's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!