{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
What are the G1, G2, G3 and Gx classifications for the ANSI Standard,...

The G3 specification references the ANSI Standard, ANSI/ISA S71.04-1985, “Environmental Conditions for Process Measurement and Control Systems: Airborne Contaminants,” . The G reference refers to the...

What does 1 way, 2 way and intermediate light switching mean?

There are 3 basic types of switches that are used for domestic purposes: 1 Way Switches: If a light switch is ‘1 way’ this means it is just an on/off switch. This is the simplest type of switch that...

PLC different memory usages in EcoStruxure Control Expert explained

The memory usage function is used to view : The physical distribution of the controller memory (see EcoStruxure™ Control Expert, Program Languages and Structure, Reference Manual) (internal memory...

PowerLogic PM3000 Series (PM3200, PM3210, PM3250, PM3255) Installation and...

Issue PM3000 Series Installation and User Guide Product Line PM3200, PM3210, PM3250, PM3255 Environment Installation, Configuration, Programming, Instruction bulletin, User Manual Cause Documentation...

Are there any standards for sizing the neutral/PE bars?

The earthing schemes and sizing differ according to the earthing scheme (TT,TN-C,TN-S,IT...etc). According to the required earthing scheme, you should size your earthing and neutral conductors. IEC...

What is the Reason of Earth leakage devices tripping without fault...

Some types of electrical and electromagnetic interference caused by the network or its environment may affect the operation of earth leakage protection devices and causes their tripping without...

What is the function of BUCHHOLZ relay in oil-filled transformers?

Buchholz protection is normally provided on all transformers fitted with a conservator. The Buchholz relay is contained in a cast housing which is connected in the pipe to the conservator, as in...

What is meant by vector group for transformers and why is it important?

What is vector group for transformers? A vector group is the International Electrotechnical Commission (IEC) method of categorizing the high voltage (HV) windings and low voltage (LV) winding...

Show more
Popular Video FAQsPopular Videos
Show more
Learn more through our Generic Knowledge FAQsGeneral Knowledge
What is meant by Symmetrical and Asymmetrical breaking currents?

issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...

In a 3 phase system, why does the meter still show voltage reading on one...

Issue: Testing phase loss on a meter doesn't result in a null voltage reading. Environmnet: EasyLogic Series Power Meters PowerLogic Series Power Meters Resolution: The voltage seen is what we...

Voltage, Current and Resistance Explained

Issue: How do I remember the relationship of voltage, current and resistance in an electrical system? Environment: N/A Solution: Voltage (unit of measurement - volt) is like the water pressure in the...

What is an Electrical "Ground Loop" - How does it affect my equipment?

Issue: What is an electrical "ground loop" and how does it affect my equipment? Environment: Ground loops can occur in any situation where multiple electrical devices are interconnected,...

Which RL(lead resistance from CT to relay) is to be used in Knee Voltage...

Issue: Having two different values for RL ( Lead resistance from the CT to the relay); RL from the phase CT to the relay and RL from the neutral point CT to the relay Environment: Protection Function...

What is Power Factor Correction (PFC) - Does it help conserve energy?

Issue: What is Power Factor Correction (PFC) - Does it help conserve energy? Answer: Explanation 1: Power Factor Correction (PFC) doesn't directly reduce the overall electric consumption of a...

Show more